Exporting the Action Object Configuration

Process+ Action Object configuration can be exported to allow users to keep a backup of the deployed loop configurations. The exported files can be used to easily redeploy the loops using the previous configuration.

Exporting Process+ Action Object

  1. Highlight the Action Object to export. Only one Action Object can be exported at a time.

  2. Click [Export] and select a place to save the files.

Export Options

File

Description

File format

Loop definition file

The loop definitions file that was used to deploy  the loops contained in the Action Object. The exported file can be used to redeploy a Process+ Action Object for the loops contained in the exported Action Object.

NOTES: The exported loop definitions file contains the Loop IDs for the deployed loops and can be used to redeploy a Process+ Action Object for the loops defined in the exported file. 

While removing an Action Object, you can either retain or delete the existing loops. Retaining the loops allows you to deploy an Action Object using this exported file without recreating the loops.

.csv file

Control mode rules

The control mode script currently in use by the Action Object.  This file can be imported by the deployment wizard when deploying or redeploying loops to define the control mode script.

Text file

Process+ backup file

The Process+ backup file contains all the configuration specified when the Action Object was deployed, with the exception of the following:

  • Process+ Action Object name

  • Number of histogram bins

  • Reporting/scheduling config (that is, the Reporting period selection)

.ProcessPlus file

 


Related topics:

  

CSense 2023- Last updated: June 24,2025